Skip to main content
tj2
Associate III
Jan 18, 2006 4:24 AM UTC
Question

ADC varying results

Posted on January 18, 2006 at 05:24

ADC varying results

This topic has been closed for replies.

5 replies

tj2
tj2Author
Associate III
Jan 17, 2006 8:51 AM UTC
Posted on January 17, 2006 at 09:51

Hi

While testing the ADC on our target board, I see that the converted result very often varies a lot or jump to a completely way off value. How can this be?

The circuit is bandwith limited to 250Hz and the prescaler is configured to a samplerate of 500Hz.

tj2
tj2Author
Associate III
Jan 17, 2006 8:59 AM UTC
Posted on January 17, 2006 at 09:59

[ This message was edited by: logic_io-TJ on 17-01-2006 14:32 ]

hichem2
Associate
Jan 18, 2006 2:59 AM UTC
Posted on January 18, 2006 at 03:59

Hi logic

As the STR71x reference manual the ADC out put result is such the attached picture.

The converted value stored in ADC_DATA[n] is a signed two’s complent value and proportional to the difference (VIN-VCM).

Can you tell me about the variation rate

And are you sure of the input source precision?

With best regards,

Hich ;)

________________

Attachments :

ADC_out_put.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtAg&d=%2Fa%2F0X0000000aJu%2F7LtrRTVx2kZbV3MkiGtPPCmhVdCpM5MbbwypflxcdPQ&asPdf=false
tj2
tj2Author
Associate III
Jan 18, 2006 3:27 AM UTC
Posted on January 18, 2006 at 04:27

Hi Hich

At one input the source is a DC power supply, trimmed to output exactly 2,500V. The other input is connected to ground through a 10k resistor (to calculate the gain and offset). Both inputs are of course bandwidth limited to 250Hz.

The variations are most of the times only a few of the LSB bits. But sometimes the converted value jumps to a completely way off value. After studying the graph you attached, I can see that what happens is that the 0V is measured to a value below zero, hence given a large (over 2.5V) value.

I've solved the problem by doing several (100) conversions , and then averaging the result.

May I ask why the ADC outputs a two's complement result? What are the benefits compared to a ''normal'' ADC?

[ This message was edited by: logic_io-TJ on 18-01-2006 08:58 ]

hichem2
Associate
Jan 18, 2006 4:24 AM UTC
Posted on January 18, 2006 at 05:24

Hi,

Normaly there is no big difference betwen a two's complement result and normal result

But there is a design chose related to the Vref value selection.

With best regards,

Hich