Skip to main content
GGrum.1197
Visitor II
November 15, 2019
Question

ADC reads a mid level value when input is floating, how can we make it read zero?

When the input to the ADC (in the STM8L151G6) is floating, it reads approximately a mid level value. For example, if the ADC's reference voltage is 3 volts it reads around 1.7 volts. Why does this happen?  We can't find a register setting that causes this to happen. We were expecting it to read 0 volts. How can we make it read 0 volts? 

    This topic has been closed for replies.

    3 replies

    Stecklo
    Senior
    November 15, 2019

    If an input is floating that means its voltage is not pulled explicitly to any level on a board. So you can't expect any specific conversion result. You could use pull-down resisor if you need zero

    Tesla DeLorean
    Guru
    November 15, 2019

    Indeed capacitor is going to need somewhere for the electrons to be going.

    Perhaps you can just commit a grounded ADC pin, and interleave to that channel before to the one that might be floating?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Stecklo
    Senior
    November 15, 2019

    Ocasionally, I have similar question.

    I'm using ADC on STM32WB55CG.

    It has no specific Vref pin, so the Vref is connected to VDDA inernally. VDDA = 3V.

    In a differential mode I have one pin always equal to 1.5V and the other one [0; 3]V. I expect the conversion result to be [-2048; 2047] or at least [0; 4096] as the ADC is 12 bit. But in fact I get about 1985 when inputs are equal and the whole range of results is somewhat [1000; 3000]

    What am I doing wrong?