Skip to main content
scott239955
Associate III
Apr 14, 2003 3:44 AM UTC
Question

ADC on ST92F150

Posted on April 14, 2003 at 05:44

ADC on ST92F150

This topic has been closed for replies.

2 replies

scott239955
Associate III
May 17, 2011 9:33 AM UTC
Posted on May 17, 2011 at 11:33

Does anyone have sample code using the ADC on the ST92F150?

Using AUTOSCAN, I noticed that it is possible to specify the channel to start the conversion, but not the channel to stop; it stops on channel Not knowing this, I used the first eight analog inputs (0 to 7) instead of 8 through If the port pins for 8 through 15 are not setup as alternate function, can the AUTOSCAN feature still be used? Will AUTOSCAN still do a conversion on analog inputs 8 through 15 even though they are not used as such?

romain2399
Associate II
May 17, 2011 9:33 AM UTC
Posted on May 17, 2011 at 11:33

I've attached an example with single mode on the Channel15, the high data register is sent by SCI_M / RS0

The AUTOSCAN starts by the defined register up to the channel Thus you must use the last contiguous channels.

The fact that you configure or not the corresponding I/Os in Analog Input Alternate Function is unknown by the ADC, it is up to you to do it.