Skip to main content
chucksoft
Associate
Mar 19, 2009 8:16 PM UTC
Question

ADC interrupt

Posted on March 19, 2009 at 21:16

ADC interrupt

This topic has been closed for replies.

4 replies

mark9
Associate III
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

Edit 91x_map.h and change the register definition for ''DDR'' to be 32 bit (see snippet), not 16 bit. I had a confirmed silicon bug regarding this from ST Micro (not in the errata) that would crash my program under weird circumstances.

...

vu32 DDR; /* ADC DMA Data Register ! NOW 32 BITS ! */

vu16 CR2; /* ADC Control Register2 */

vu16 EMPTY16;

} ADC_TypeDef;

chucksoft
chucksoftAuthor
Associate
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

Actually, for the version of code I posted, I should have said a value of 0xF3 or greater works.

chucksoft
chucksoftAuthor
Associate
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

I'm running the A/D converter in scan mode, with 7 channels enabled. Conversion mode is single. I'm using a STR912FAW44. PCLK is 48 Mhz. I field the interrupt, clear the flag, read the conversions, then start the next conversion. If I use an ADC prescaler of 0xF0 or larger, all works fine. Using a value of 0xE0 or smaller causes me to hit a small # of interrupts, then no more. Here is my code:

ADC_InitTypeDef ADC_InitStructure;

ADC_DeInit();

ADC_StructInit(&ADC_InitStructure);

ADC_InitStructure.ADC_Channel_0_Mode = ADC_NoThreshold_Conversion;

ADC_InitStructure.ADC_Channel_1_Mode = ADC_NoThreshold_Conversion;

ADC_InitStructure.ADC_Channel_2_Mode = ADC_NoThreshold_Conversion;

ADC_InitStructure.ADC_Channel_3_Mode = ADC_NoThreshold_Conversion;

ADC_InitStructure.ADC_Channel_4_Mode = ADC_NoThreshold_Conversion;

ADC_InitStructure.ADC_Channel_5_Mode = ADC_NoThreshold_Conversion;

ADC_InitStructure.ADC_Channel_6_Mode = ADC_NoThreshold_Conversion;

ADC_InitStructure.ADC_Scan_Mode = ENABLE;

ADC_InitStructure.ADC_Conversion_Mode = ADC_Single_Mode;

ADC_Cmd(ENABLE);

ADC_PrescalerConfig(0x80);

ADC_Init(&ADC_InitStructure);

VIC_Config(ADC_ITLine, VIC_IRQ, ADC_PRI);

VIC_ITCmd(ADC_ITLine, ENABLE);

ADC_ITConfig(ADC_IT_ECV, ENABLE);

ADC_ConversionCmd(ADC_Conversion_Start);

void ADCIsr(void)

{

int i;

ADC_ClearFlag(ADC_FLAG_ECV); //clear the interrupt

for(i = 0;i < 7;i++)

Conversion_Value[i] = ADC_GetConversionValue(i);

NewConversionReady = 1;

ADC_ConversionCmd(ADC_Conversion_Start);

}

If I add some code in the ISR between clearing the flag and starting the next conversion to slow things down, I can get away with smaller values of the prescaler...down to 0xA0.

Any idea what is going on?

Thanks,

Chuck Smith

chucksoft
chucksoftAuthor
Associate
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

Hi Lakata,

Thanks for the feedback. I took a look at 91x_map.h, but mine doesn't have

the DDR and CR2 fields - my last field is the PRS. I am not using the DMA on the ADC, so I guess that's why I haven't noticed before. I thought I had the latest version of the firmware library, but maybe a more recent one has been released.

Chuck