Skip to main content
sjackson
Associate III
Dec 13, 2007 6:22 AM UTC
Question

ADC Input Impedance

Posted on December 13, 2007 at 07:22

ADC Input Impedance

This topic has been closed for replies.

3 replies

sjackson
sjacksonAuthor
Associate III
May 17, 2011 7:43 AM UTC
Posted on May 17, 2011 at 09:43

Where can I find a spec for the input impedance of the ADC on the STR912?

I've looked in the datasheet but don't see it anywhere (one would expect to see it in the ''ADC Electrical Characteristics'' section).

Thanks.

claus
Visitor II
May 17, 2011 7:43 AM UTC
Posted on May 17, 2011 at 09:43

I asked the tech Support..

If AD-Input-Voltage is in the range 0V..VDDQ: Rin> 100MOhm, Cin = 5pF

ocean_front_view
Visitor II
May 17, 2011 7:43 AM UTC
Posted on May 17, 2011 at 09:43

Can a ST applications engineer please answer this question. This is a very standard spec. that should be in the data sheets.

FYI I measure 1.3uA.