Skip to main content
butler_gaoyh
Associate
Oct 12, 2005 11:23 PM UTC
Question

about the str730's sram

Posted on October 13, 2005 at 01:23

about the str730's sram

This topic has been closed for replies.

5 replies

butler_gaoyh
Associate
Oct 10, 2005 10:08 AM UTC
Posted on October 10, 2005 at 12:08

there only 16K bytes sram with str730,but in fact it is too little to use it in the products,so i want to konw how to extend the sram without emi?

hichem2
Associate
Oct 11, 2005 3:23 AM UTC
Posted on October 11, 2005 at 05:23

Hi,

STR73x features 16 KBytes of static RAM and I don't think that you can extend the sram size without emi.

Best regards,

Hich ;)

[ This message was edited by: Hich on 12-10-2005 15:44 ]

butler_gaoyh
Associate
Oct 12, 2005 8:25 AM UTC
Posted on October 12, 2005 at 10:25

thanks for Hich 's reply.

i cared for st's arm just because it has four uarts and enough capacity flash to me,but with too little of sram,so maybe i don't think it as a good design.

everybody can image a mcu with so many functions,but only 16k sram.maybe it is a mistake of st.

hichem2
Associate
Oct 12, 2005 9:55 AM UTC
Posted on October 12, 2005 at 11:55

Hi butler,

my be only 16k of sram is not a very good Feature in our device

But can you tell me which kind of application need more than 16K.

regards,

Hich :o

butler_gaoyh
Associate
Oct 12, 2005 11:23 PM UTC
Posted on October 13, 2005 at 01:23

Hi Hich,

First i think it is a question without the answer 'yes' or 'no'.One MCU only can do something,not everything.

just for power monitor system,our products will communction with the devices,such as power supply,air-condition and so on,each devices needs more than 4k's ram for buffer and data.the 16k is little without the func of iap,can,and usb.

maybe someone else has the same idea as me,only i speak out. why? just because i care st's str7.