Skip to main content
達井上.1
Associate
October 4, 2021
Question

About M95160

Does POR work even if the power is turned on slowly (even if the rise time is slow)?

No rise time is specified in the data sheet. 

This topic has been closed for replies.

2 replies

Mike_ST
ST Technical Moderator
October 4, 2021

Hello,

I don't see any restriction on that:

"5.1.2

At power-up, the device does not

respond to any instruction until VCC reaches the POR threshold voltage."

My interpretation is that there no time out for the POR feature.

The only constraint on VCC that I can see:

"5.1.3

The VCC voltage has to rise continuously from 0 V up to the minimum VCC operating voltage

defined under Operating conditions in Section 9."

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
達井上.1
Associate
October 5, 2021

Hello,​

​

Thank you for your reply.

​

Constraints pointed out 5.1.3

I think

"Continuous" = If the rising voltage does not increase or decrease temporarily due to noise etc.