Associate III
May 24, 2025
Solved
A6727 design concern
- 6 replies
- 857 views
I'm using E Design Suite to build a buck (step-down) converter circuit and would like to know if there's anything in the design that I should be concerned about. I've reviewed the schematics in the datasheets, and they seem to be about the same.
I plan to use the same MOSFET model for both the high-side and low-side switches to simplify component sourcing. Could this be a problem?
I intend to use this circuit to power several servos, so the output should provide at least 10 A. Should I add more capacitors at the output? Would it also be a good idea to include flyback diodes?
The link to the simulation: link