Skip to main content
TFei.1
Visitor II
May 4, 2020
Question

A liker error when adding ADC && UART to STM8S_TouchSensing_Lib_V2.5.0 example project

I downloaded the STM8S_TouchSensing_Lib_V2.5.0 , and the function of touch sensing key has been done completley.

Now i'd like to add the adc && uart based on the current project, you can see the detail on the attachment, but there will be a linker error as below

"Error[Li005]: no definition for "assert_failed" [referenced from E:\Work\Code\STM8S_TouchSensing_Lib_V2.5.0\Projects\Examples\STM8S207K6_Ex02_Heat\EWSTM8\Debug\Obj\stm8s_uart1.o] "

"Error while running Linker "

Would you please help me check how to correct it?

Best Regards,

Fei

    This topic has been closed for replies.