Skip to main content
shangdawei1
Associate III
Oct 10, 2005 4:12 AM UTC
Question

4MHz to 48MHz for USB at STR711

Posted on October 10, 2005 at 06:12

4MHz to 48MHz for USB at STR711

This topic has been closed for replies.

3 replies

shangdawei1
Associate III
Oct 10, 2005 1:09 AM UTC
Posted on October 10, 2005 at 03:09

see:

http://www.olimex.com/dev/pdf/str-p711.pdf

Only 4MHz in sch for CK, and I can not find 48 MHz for USBCLK(P1.10). USBCLK(P1.10) is used to check SD card.

4MHz Clock to HCLK(P1.13) for HDLC. can HCLK uses as USB clock?

if it can , how can i setup ?

ben2
Associate III
Oct 10, 2005 2:56 AM UTC
Posted on October 10, 2005 at 04:56

yes you can feed 4Mhz into the HCLK and use this for the USB clock. This is what I am doing. You just need to setup PLL2CR register.

/* setup clock */

PCU->PLL2CR = 0x0050; /* x12 /1 */

while( (PCU->PLL2CR & 0x8000) == 0) { /* wait for pll to lock */

asm(''nop'');

};

PCU->PLL2CR |= 0x0180; /* enable pll output and to use as usb clock */

Doing this means the HDLC and USB share the same clock.

shangdawei1
Associate III
Oct 10, 2005 4:12 AM UTC
Posted on October 10, 2005 at 06:12

Quote:

On 10-10-2005 at 08:26, Anonymous wrote:

yes you can feed 4Mhz into the HCLK and use this for the USB clock. This is what I am doing. You just need to setup PLL2CR register.

/* setup clock */

PCU->PLL2CR = 0x0050; /* x12 /1 */

while( (PCU->PLL2CR & 0x8000) == 0) { /* wait for pll to lock */

asm(''nop'');

};

PCU->PLL2CR |= 0x0180; /* enable pll output and to use as usb clock */

Doing this means the HDLC and USB share the same clock.

Thanks, i understand now