Skip to main content
tnn1985
Associate II
Mar 17, 2011 12:19 PM UTC
Question

16bit SPI on STM8

Posted on March 17, 2011 at 13:19

16bit SPI on STM8

    This topic has been closed for replies.

    4 replies

    tnn1985
    tnn1985Author
    Associate II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Seems like nobody can help me with that. I also tried BitBanging but it doesnt work either.

    tnn1985
    tnn1985Author
    Associate II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Ok, this should work. I guess the problem was that the interna Clockl f_Master was set to Clock/8 by default (HSIDIV = 8). My application has a SPI-Frequency of 2Mhz. The problem is that the highest frequency of SPI can only set to f_Master/2, which means i could only reach 1Mhz. I switched to 16Mhz High Speed External Oscillator no Prescaler to solve this problem.

     while (SPI_GetFlagStatus(SPI_FLAG_TXE) == RESET) lines need to be uncommented!!!

    tnn1985
    tnn1985Author
    Associate II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Hi,

    actually i want to write something TO the Master. If i send something like :

    void sendValue (signed short int value)

    {

        unsigned char UpperByte = (unsigned char) (value >> 8);

        unsigned char LowerByte = (unsigned char) (value >> 0);

        //Value is Transmitted in bit 14:3

    //    while (SPI_GetFlagStatus(SPI_FLAG_TXE) == RESET);

        //!!!!!first bit (bit 15) doesnt care)

        SPI_SendData(UpperByte);

    //    while (SPI_GetFlagStatus(SPI_FLAG_TXE) == RESET);

        //!!!!!last three bits (bit 2:0) doesnt care)

        SPI_SendData(LowerByte);

       

    }

    it sends the UpperByte twice. One time in the first 8 clock cycles and the second time in the second 8 clock cycles.

    fggnrc2
    Associate III
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Hello tnn!

    Some years ago, I read this ST7 Application Note

    http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/APPLICATION_NOTE/CD00004301.pdf

    which should work for STM8 too.

    I hope it could help you...

    EtaPhi