Skip to main content
balaji_softproff
Associate III
Feb 17, 2006 11:56 AM UTC
Question

128 mbits RAM and STPC atlas

Posted on February 17, 2006 at 12:56

128 mbits RAM and STPC atlas

This topic has been closed for replies.

5 replies

balaji_softproff
Associate III
Nov 14, 2005 6:34 AM UTC
Posted on November 14, 2005 at 07:34

Hai,

Could anyone tell me how to configure STPC atlas for onboard RAM chips of 128mbits. (by default it is configured for 64mbits).

thanks in advance

Balaji

kaouther
Associate II
Nov 17, 2005 9:10 AM UTC
Posted on November 17, 2005 at 10:10

Hi,

The default configuration is 64 Mbits or 128 Mbits 4 SDRAM 4 banks and it should work for your case. There is no config only for th 128Mbit.

You have two possibilities with 128Mbit configuration.

Reg 084C6008:00000002;64 Mbits or 128 Mbits 4 SDRAM banks.

Reg 084C6008:00000001; 64 Mbits or 128 Mbits 2 SDRAM banks.

Regards.

balaji_softproff
Associate III
Nov 18, 2005 3:55 AM UTC
Posted on November 18, 2005 at 04:55

thanks for your reply,

Actually I want to use a 128 MB DIMM Ram , which has eight 128Mbits chips. Now I donot want to use the onboard 64MB memories,

also can i load linux in protected mode with L1(onchip cache) disabled

Could you help me with this.

Thanks in advance

Balaji

[ This message was edited by: balsara on 19-11-2005 10:45 ]

balaji_softproff
Associate III
Nov 30, 2005 7:46 AM UTC
Posted on November 30, 2005 at 08:46

hello sir

My aim is to replace the onboard memory of stpc evaluvation kit with DIMM socket. But if i do so, my program executes in shadow region and not outside it.

To make a ljmp in protected mode i need the cache or hidden registers (On chip cache register) which have the access details of that region.

can you suggest me what i should do to make my cache working.

please atleast guide me to any article regarding this

thanks in advance

Balaji

kaouther
Associate II
Feb 17, 2006 11:56 AM UTC
Posted on February 17, 2006 at 12:56

Did you loked to the cache register in the Vega programming manual?

Also you can have a look to the bios writer's guide.

For the use of DIMM ram and not the onboard chip, if you are using our evaluation board you can select either the DIMM or the soldred chip via jumpers P713, P712, P711 and P710. PLease refer to the evaluation boars user manual for jumper settings.

You can download thes documpents from the web site.

Regards.