Skip to main content
knisbet
Associate II
April 30, 2004
Question

1024x768 24 bit color on STPC Industrial

  • April 30, 2004
  • 2 replies
  • 795 views
Posted on April 30, 2004 at 18:15

1024x768 24 bit color on STPC Industrial

This topic has been closed for replies.

2 replies

knisbet
knisbetAuthor
Associate II
April 13, 2004
Posted on April 13, 2004 at 11:32

Is the STPC Industrial capable of operating in 1024x768 24 bit color mode? I believe this is mode 0x118. Vmode does not work in this mode, but I don't know if it is a limitation of vmode or of the VGA controller.

Thanks
marios
Associate III
April 30, 2004
Posted on April 30, 2004 at 18:15

This mode is not supported by the Windows driver either. But even at 1024-768x16bpp, the power consumption and temperature rise become a concern. It would get worse at 32bpp.

I wonder if the Atlas supports it.