Skip to main content
Amelie ACKERMANN
ST Community Manager
September 23, 2024

Flexible, space-saving class-D amplifier for in-car audio adds automotive-optimized diagnostics

Related products:Other hardware and tools

The HFA80A automotive-grade analog-input class-D audio amplifier combines high efficiency, small size, and a low bill of materials, with load diagnostics optimized for automotive and native electromagnetic compatibility (EMC).
 

With its feedback-before-filter topology and 2MHz nominal PWM frequency, the HFA80A lets designers optimize the output filter for the targeted performance and achieve a compact outline with small component values. Spread-spectrum operation simplifies meeting the mandatory CISPR 25 specification, with no additional EMC-specific filtering required.
 

The amplifier delivers clear and powerful listening experiences, driving up to 4x 49W into 2Ω speakers at 14.4V and with typical harmonic distortion (THD) specified at 0.015% (1W/4Ω). Pure sound is assured, with low output noise and crosstalk as well as 80dB power supply rejection specified at 1W/1kHz with 4Ω loads.
 

Flat frequency response up to 40kHz ensures generous bandwidth for high-resolution audio, which designers can extend to 80kHz by optimizing the filter. In addition, the HFA80A can handle performance-centric applications such as noise cancelling thanks to low latency by design.

 

The automotive-specific diagnostics is based on a specially conceived noise-immune algorithm capable of detecting anomalous load conditions and variations. Features include independent DC and AC load detection for each channel, detection of short-circuit on startup, and overcurrent protection with configurable thresholds. Further diagnostic checks include input-voltage DC-offset detection, output-current offset detection, and thermal protection with a choice of four different thermal warnings.
 

A dedicated, configurable pin signals the host microcontroller when new diagnostic information is available, which simplifies host communications and relieves CPU workload. An I2C-bus interface provides access to the device features and diagnostic data, and a backup mode lets the amplifier continue operating even if I2C control is lost. In addition, the HFA80A features a digital admittance meter (DAM) that eases development by helping engineers check the connected speaker characteristics without external measurement tools or sensors.
 

The HFA80A is available now in a compact 7mm x 7mm LQFP48L thermally enhanced package with exposed pads, from $4.80 for orders of 1000 pieces.
 

Additional resources

First published on Sep 23, 2024

11 replies

Visitor II
September 23, 2024

Sounds like a cool audio amplifier. Thanks for sharing. 

ST Employee
October 17, 2024

A very well born amplifier calling for complementary talented family members ... More to come for sure ...

Explorer II
November 7, 2024

Seems very nice class D with 2MHz pwm...

mladen
Associate II
November 8, 2024

Hi !

Is there a evaluation boards boards for HFA80A?

Amelie ACKERMANN
ST Community Manager
November 12, 2024

Hello @mladen ,

Yes, there is a demo board, the ordering code is EVAL-HFA80A-SA. However, the board can only be ordered through authorized distributors (not e-commerce distributors). You find a list of distributors across regions here: Contacts - STMicroelectronics

I hope this helped. Let me know if there is anything else. 

Best,

Amelie

 

Visitor II
April 14, 2025

Hello, I have just bought a few HFA80A, but i cannot get it to amplifier.. actually using 1chln, only.. but we need more documentation to make it work... im doing a 32khz by arduino pwm at 2,56V in CHLN1, supply it with 10V, following the steps in the data? we need to know, if this HFA80A ll work for our products.

Salutes

Amelie ACKERMANN
ST Community Manager
April 16, 2025

Hello @felipegz94 ,

Thank you for getting in touch. I reached out to the responsible team to see how we can help sort out your issue. I will be in touch again as soon as possible. 

Best,

Amelie

Amelie ACKERMANN
ST Community Manager
April 22, 2025

Hello @felipegz94 ,

to receive the respective documentation to help sort the issue, please reach out to the local ST sales office or distributor in your country/region. You find list of offices here: Contacts - STMicroelectronics

I hope this helps!

Best,

Amelie

Visitor II
August 27, 2025

Hello!  

1) Can HFA80A bridge four channels and then parallel them into two or one channel? If feasible, is there any reference?

2) Is his frequency 2M fixed internally or can the frequency be changed externally by modifying resistors or capacitors?

Thank you!

Visitor II
August 27, 2025

Where can I download EVAL-HFA80A-SA?