Skip to main content
t.saito
Associate
Oct 18, 2018 1:05 AM UTC
Solved

Zero-g level offset of LIS2DH12 at FS bit set to '11', and Normal resolution mode.

LIS2DH12, Zero-g level offset is 40mg at FS bit set to '00'.

When using the FS bit set to '11' and Normal resolution mode, what value is it?

40mg * 12 = 480mg ?

or

40mg * 48 = 1920mg?

    This topic has been closed for replies.
    Miroslav BATEKBest answer
    ST Employee
    Oct 22, 2018 12:40 PM UTC

    ST doesn't specify this value.

    But I would expect that if the zero-g level at FS=2g is typically 40mg, for FS=16g it could be 8-times higher.

    4 replies

    Miroslav BATEKBest answer
    ST Employee
    Oct 22, 2018 12:40 PM UTC

    ST doesn't specify this value.

    But I would expect that if the zero-g level at FS=2g is typically 40mg, for FS=16g it could be 8-times higher.

    t.saito
    t.saitoAuthor
    Associate
    Oct 23, 2018 12:28 AM UTC

    Dear Miroslav BATEK,

    Thank you for your reply.

    But, I don't understand if zero-g level offset is affected by resolution mode(High resolution or Normal or Low-power).

    Do not I have to worry about the resolution mode?

    ST Employee
    Oct 24, 2018 7:50 AM UTC

    I don't think the resolution will have significant impact on the zero-g level.

    t.saito
    t.saitoAuthor
    Associate
    Oct 24, 2018 9:12 AM UTC

    Dear Miroslav BATEK.

    Thank you!

    Your answer was very helpful.