Skip to main content
Kabron
Associate II
January 21, 2019
Question

X-NUCLEO-53L0A1 and VL53L1X problem

Hello, I have X-NUCLEO-53L0A1 kit and now I want to work with VL53L1X sensors using this kit. As I understand, the only differences between X-NUCLEO-53L0A1 and X-NUCLEO-53L1A1 are:

1. Different top sensor component

2. Absence of 4 digit display on X-NUCLEO-53L1A1.

So, if I disable top sensor by grounding XSHUT_2.8V signal, I'll could work with left and right sensors VL53L1X, placed on CONN LEFT and CONN RIGHT. And it really works, but with the following limitation:

I have to initially disconnect XSHUT_L and XSHUT_R signals before launching VL53L1X_GUI, because these signals are kept low on GUI startup and the SW could not find any sensor. If after startup I reconnect these signals, everything works fine.

The question is what is the reason of such strange behaviour? And what could be done to solve the problem?

Thanks in advance,

Vladimir

    This topic has been closed for replies.