Skip to main content
MMa.1893
Associate III
November 2, 2020
Question

X-CUBE-MEMS1 lib for other sensor? This library is intended to work with ST MEMS only.

most of X-CUBE-MEMS1 lib said :"This library is intended to work with ST MEMS only."

It is true? i'm use LSM9DS1 that not supported by X-CUBE_MEMS1.

So, Can i Use X-CUBE_mems lib for this sensor(or even not ST sensor?)

Thank you!

    This topic has been closed for replies.

    2 replies

    MMa.1893
    MMa.1893Author
    Associate III
    November 3, 2020

    anybody?

    Eleon BORLINI
    ST Employee
    November 3, 2020

    Hi @MMa.1893​ ,

    please note first of all that the X-CUBE-MEMS1 libraries are designed to be compliant with ST sensors, meaning that the all the device register configurations, the I2C/SPI communication and the combination of sensors in the applications are designed on ST sensors.

    You might intend to use the same algorithms for other than ST sensors, but please note that the algorithm source codes are not open and you should contact an STMicroelectronics sales office representatives for further information, since the release of STM proprietary libraries is subject to signature of a License User Agreement (LUA).

    With specific regards to the LSM9DS1 device, I agree with you that there are no examples for this specific sensor in the X-CUBE-MEMS1 libraries.

    But you could include in a CubeMX project or in an already existing application code the C drivers you can find on Github repository, at this link.

    -Eleon