Skip to main content
RAbra.2
Associate
June 26, 2020
Question

Wrong x,y and z first sample for LIS331DLH after configuration change?

I am using a LIS331DLH accelerometer chip and I have seen that when I change its configured sometimes I get double value for x, y and z but only for the first sample. Do I need to discard the first sample after configuration change like some other chips?

I am changing from 2G to 8G configuration and sample is as follows:

1st sample:

x: 26

y: 8

z: 521

2nd sample onwards:

x: 13 (+- 5)

y: 1 (+- 5)

z: 261 (+- 5)

    This topic has been closed for replies.

    5 replies

    Eleon BORLINI
    ST Employee
    June 29, 2020

    Hi @RAbra.2​ , this should not be the case... Did you try with setting the Block data update (BDU) bit in register CTRL_REG4 (23h)? This sets the output registers not updated between MSB and LSB reading. Well when do you perform the self test it is always suggested to discard the first sample, but not in the normal mode running. If however you can afford to discard the first sample after the power on, especially if you uses high ODRs, you could discard the first value or at least apply on it a moving average. Regards

    RAbra.2
    RAbra.2Author
    Associate
    June 30, 2020

    HI @Eleon BORLINI​ 

    We are setting BDU bit in CTRL_REG4. Here is our CTRL_REG4 configuration:

    CTRL_REG4.bits.BDU = 1;

    CTRL_REG4.bits.BLE = 0;

    CTRL_REG4.bits.FS = target_fullscale_selection;

    CTRL_REG4.bits.STsign = 0;

    CTRL_REG4.bits.ST = 0;

    CTRL_REG4.bits.SIM = 0;

    As you can see only FS bits are changeable in our configuration. We cannot apply a moving average at it this moment in our project as it might impact the scope but we can afford to discard the first sample if it is the only solution available. Kindly confirm.

    NOTE: In all configuration we are using ODR = 50 Hz.

    Regards

    RAbra.2
    RAbra.2Author
    Associate
    July 14, 2020

    @Community Admin​  @Eleon BORLINI​ 

    Can you please provide a confirmation on the above?

    Regards

    Eleon BORLINI
    ST Employee
    July 14, 2020

    Hi @RAbra.2​ , I suggest you to refer to the online C drivers on Github, lis331dlh_reg.c. The BDU bit can be managed as follows:

    /**
     * @brief Block data update.[set]
     *
     * @param ctx read / write interface definitions(ptr)
     * @param val change the values of bdu in reg CTRL_REG4
     *
     */
    int32_t lis331dlh_block_data_update_set(stmdev_ctx_t *ctx, uint8_t val)
    {
     lis331dlh_ctrl_reg4_t ctrl_reg4;
     int32_t ret;
     
     ret = lis331dlh_read_reg(ctx, LIS331DLH_CTRL_REG4, (uint8_t*)&ctrl_reg4, 1);
     if(ret == 0) {
     ctrl_reg4.bdu = val;
     ret = lis331dlh_write_reg(ctx, LIS331DLH_CTRL_REG4,
     (uint8_t*)&ctrl_reg4, 1);
     }
     return ret;
    }
     
    /**
     * @brief Block data update.[get]
     *
     * @param ctx read / write interface definitions(ptr)
     * @param val change the values of bdu in reg CTRL_REG4
     *
     */
    int32_t lis331dlh_block_data_update_get(stmdev_ctx_t *ctx, uint8_t *val)
    {
     lis331dlh_ctrl_reg4_t ctrl_reg4;
     int32_t ret;
     
     ret = lis331dlh_read_reg(ctx, LIS331DLH_CTRL_REG4, (uint8_t*)&ctrl_reg4, 1);
     *val = ctrl_reg4.bdu;
     
     return ret;
    }

    Btw, if you can discard the first sample of the acquisition, I suggest you to do this (this is in general a good practice, because the first data samples could be affected by startup effects both electrical and mechanical that may be due to the environment).

    Regards

    RAbra.2
    RAbra.2Author
    Associate
    July 14, 2020

    @Eleon BORLINI​ 

    Thank you for the information. We shall proceed accordingly.

    Regards