Skip to main content
TStee.1
Visitor II
March 14, 2023
Question

Wrist tilt and "funny" data in FUNC_SRC2

Hi,

I trying to get the wrist tilt working. I have used the example in AN5040 page 55.

I using the simple example setup, nothing else is set.

  • Write 20h to CTRL1_XL
  • Write 84h to CTRL10_C
  • Write 01h to DRDY_PULSE_CFG

When reading the FUNC_SRC2 it always returns 0x84 which should be impossible according to datasheet. The bit WRIST_TILT_IA never goes high no matter how much the unit is tilted.

I have already have accelerometer and gyroscope with FIFO and up and running so my drivers and the chip are working. However this I have disabled and are using only the 3 commands above.

What am I missing, any ideas?

Thanks

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
April 12, 2023

Hi @TStee.1​ ,

Have you already tried the complete procedure,to be repeated when the accelerometer exits from Power-Down mode, described in AN5040?

1. Write 20h to CTRL1_XL // Turn on the accelerometer // ODR_XL = 26 Hz, FS_XL = ±2 g

2. Write 04h to CTRL10_C // Enable embedded functions

3. Wait 50 ms

4. Write 00h to CTRL10_C // Disable embedded functions

5. Write A0h to FUNC_CFG_ACCESS // Enable access to embedded registers (bank B)

6. Set new latency in A_WRIST_TILT_LAT

7. Set new threshold in A_WRIST_TILT_THS

8. Set new mask in A_WRIST_TILT_Mask

9. Write 00h to FUNC_CFG_ACCESS // Disable access to embedded registers (bank B)

10. Write 84h to CTRL10_C // Enable embedded functions // Enable AWT detection

11. Write 01h to DRDY_PULSE_CFG // AWT interrupt driven to the INT2 pin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.