Skip to main content
falling_in2_infinity
Associate II
April 26, 2022
Question

Which MCUs have SAI with PDM interface, as suggested by AN5027?

I'm trying to implement a 6- or 8-microphone arrangement, as outlined in AN5027 (p25). The recommended approach is to use an SAI with PDM interface, but I'm struggling to find a suitable MCU (and subsequently, a suitable Nucleo dev board).

I've not even seen an actual working example of this, but I'm assuming I'd configure the PDM as a mode in the SAI configuration. What I know for sure is that when I configure the SAI on my L4A6ZG, there is no option for PDM mode.

I'd welcome any advice.

Thanks!

This topic has been closed for replies.

7 replies

Walid ZRELLI
Visitor II
April 26, 2022

Hello @falling_in2_infinity​ ,

We provide many examples that use an SAI with a PDM interface.

You can refer to the following examples provided under the H7 Firmware Package:

  • Path: Firmware\Projects\STM32H743I-EVAL\Examples\BSP
  • Path: Firmware\Projects\STM32H735G-DK\Examples\BSP
  • Path: Firmware\Projects\STM32H743I-EVAL\Examples\SAI\SAI_AudioPlayback

I hope this helps.

BeST Regards,

Walid

falling_in2_infinity
Associate II
April 26, 2022

Thanks Walid,

That's great, thanks! So other than the H7, which other MCUs have a PDM interface? Is there a simple way to find products with a given interface? The product selector page doesn't seem to allow this level of filtering.

Thanks,

...Joe.

Walid ZRELLI
Visitor II
April 27, 2022

Hello @falling_in2_infinity​ 

Take a look at the following MCUs which have a PDM interface: F2/F4/F7/H7/WB

BeST Regards,

Walid

waclawek.jan
Super User
April 26, 2022

Have a look at 'G4, the L4+ (i.e. the higher-end L4 with letters in the numbering), and maybe 'L5/'U5?

We are begging ST for ages to produce a comprehensive overview of modules' versions across the various families.

JW

falling_in2_infinity
Associate II
April 27, 2022

Thanks JW. I'll check these out.

I join your campain to ST... it's very strange not to have such an overview. I would not even mind if more features were searchable in the product finder.

...Joe.