Skip to main content
Sjito
Associate
Jul 4, 2019 4:54 AM UTC
Solved

Which document has instructions about top mark of LSM303AH chip?Looking forward to your reply. Thank you.

..

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Jul 5, 2019 7:12 AM UTC

​@Sjito​ yes, It should be a LSM303AH. The "903" refers to the year and to the week "YWW", while "03A" is part of the name "LSM303AH". Btw, you can be sure it's a LSM303AH checking the WHO_AM_I_A (0Fh) register via SPI/I2C and receiving 43h. Regards

7 replies

Eleon BORLINI
ST Employee
Jul 4, 2019 9:22 AM UTC

Hi @Sjito​ , which is the purpose for this request about device marking? Do you need the meaning of the info on the top side of the marking? They are related to the process flow of the single device, from assembly to finishing. Regards

Sjito
SjitoAuthor
Associate
Jul 4, 2019 11:22 AM UTC
  • Thanks for your reply. I just want to judge whether the chip I bought is LSM303AH through the TOP MARK. I checked the data sheet of LSM303AH, but could not find anything about it.