Skip to main content
waclawek.jan
Super User
Sep 7, 2020 5:30 PM UTC
Solved

Where to buy the 5x MEMS Mic module MB1299?

This module is advertised in manuals to several ST development boards, e.g. the 'F413 Disco.

Why is there no product folder for this module?

JW

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Sep 9, 2020 9:57 AM UTC

    Hi @Community member​ ,

    after internal double-check, I can confirm you that MB1299 mic module is provided exclusively in conjunction with the eval kit. I agree with you it should be specified...

    Please note that the MP34DT01-M on the MB1299 is not the best-in-class MEMS mic in ST portfolio, and that the optimized design for the beamforming app is the Bluecoin one.

    -Eleon

    4 replies

    Eleon BORLINI
    ST Employee
    Sep 8, 2020 3:04 PM UTC

    Hello @Community member​ ,

    I'm afraid this module has to be bought together with the entire dev kits... but currently I'm checking internally to be sure of my statement.

    Please consider that the suggested setup (HW+SW) for the beamforming app with STM MEMS microphone is the STEVAL-BCNKT01V1.

    -Eleon

    waclawek.jan
    Super User
    Sep 8, 2020 3:32 PM UTC

    Hi @Eleon BORLINI​ ,

    Thanks for the answer.

    > I'm afraid this module has to be bought together with the entire dev kits...

    Which dev kits?

    Does it come bundled with the 'F413 DISCO? Are you sure?

    The 'F413 Disco databrief nor manual says so, both mention only "Expansion connectors:– Audio daughterboard (5 ST-MEMS microphones)". The module is not on the pictures. I can't find anything on the webfolder to that kit either, idicating that this module is bundled.

    Can you please verify this information?

    Thanks,

    JW

    Eleon BORLINI
    ST Employee
    Sep 8, 2020 3:38 PM UTC

    Hi @Community member​ ,

    >> Which dev kits?

    I was referring to the STM32H7B3I-EVAL kit, but I'm verifying with my colleagues from MCU division since the module it was developed a few years ago.

    I'll keep you updated and give a feedback as soon as possible.

    -Eleon

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Sep 9, 2020 9:57 AM UTC

    Hi @Community member​ ,

    after internal double-check, I can confirm you that MB1299 mic module is provided exclusively in conjunction with the eval kit. I agree with you it should be specified...

    Please note that the MP34DT01-M on the MB1299 is not the best-in-class MEMS mic in ST portfolio, and that the optimized design for the beamforming app is the Bluecoin one.

    -Eleon