Skip to main content
Cédric Caron
Associate
March 13, 2018
Question

When will the VL53L1X API source code be available

Posted on March 13, 2018 at 09:31

The default application

http://www.st.com/content/st_com/en/products/embedded-software/proximity-sensors-software/stsw-img008.html

doesn't allow to use the multi-zone feature mentionned in this

http://www.st.com/content/st_com/en/about/media-center/press-item.html/p3918.html

. I believe I'll need to wait for the API source code to be released to get access to this feature. It turns out that as of today, there is no download available on this

http://www.st.com/content/st_com/en/products/embedded-software/proximity-sensors-software/stsw-img007.html

.

Can I get an idea on when such code will be released ?

Thank

#vl53l1
This topic has been closed for replies.

5 replies

artgodwin
Associate II
April 13, 2018
Posted on April 13, 2018 at 02:14

It is on that page (or, perhaps it is once again on that page).

At the bottom, on the right, is a blue box marked 'get software'. Click that and you get a license agreement and then a link to the actual download.

If you can't see that box, it's probably a javascript issue or something.

Cédric Caron
Associate
April 19, 2018
Posted on April 19, 2018 at 10:58

Thank you for your answer. I confirm that the link was not on the page when I created this post.

John E KVAM
ST Employee
May 1, 2018
Posted on May 02, 2018 at 00:54

No, you didn't make a mistake. Someone at ST detected a bug and the code removed until it was fixed. If you get a chance re-download the latest. They tell me it was a minor issue, but they were worried about it.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
adrian godwin
Visitor II
May 2, 2018
Posted on May 02, 2018 at 03:11

Do you think it would be possible to provide a little more detail in the release note than

'

- SLA0081 Headers harmonisation.

- Identical macro names conflict between VL53L1X and VL53L0X fix.

'

There are nearly 7000 lines of differences between the two versions (ignoring the change to directory layout) and while a large amount of that is copyright notices, there are still quite a lot of obscure changes.

I submitted a bug report consisting of 16 errors resulting in total loss of data. I haven't worked out yet whether the changes address the faults I found, but I haven't even had an acknowledgement yet. So I'd wait for the next version if I were you.

chetan sarma
Visitor II
June 13, 2018
Posted on June 13, 2018 at 07:48

Yea ,when I had gone through the document about STSW-IMG007 ,it is mentioned there is a folder for Apiexample under Api which is not in the STSW-IMG007.zip file .When will it be updated?

When will VL53L1X linux library will be released?

Thanks in advance