Skip to main content
PQiu.1
Visitor II
July 23, 2020
Question

What's the minimum target size for VL53L1X and VL53L3CX ?

Hi, i want to use VL53L1X and VL53L3CX  to detect a small size target (e.g finger,rope) at 1 meter away. i am wandering what's the minimum target size for VL53L1X and VL53L3CX ?

Thanks.

    This topic has been closed for replies.

    1 reply

    Julien NGUYEN
    ST Employee
    July 23, 2020

    Hi

    A finger at 1 m will be difficult to detect, actually the surface is too small and the distance is too long to have enough photons coming back even if the human skill has a quite good IR refelectance ~60%. Anyway, you have better chance with the L1X and the L3CX because the L1X has lens so better sensitivity. Just try it.

    Thanks,

    Julien

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.