Skip to main content
ABara.9
Associate
August 20, 2018
Question

What is the time required by the STLM20 between the application of supply voltage and valid Vout? My test results suggest 2ms but was hoping to see a published value in the datasheet.

..

This topic has been closed for replies.

2 replies

ST Employee
August 21, 2018

What you mean by valid Vout? It is very difficult to define such a parameter.

The time will be dependent on the load capacity, temperature change, thermal capacity of your HW, ...

ABara.9
ABara.9Author
Associate
August 22, 2018

By valid Vout, I mean a Vout that represents current temperature reading. When supply voltage is applied, there is a steadily increasing voltage at Vout that ultimately settles at a level that represents the current temperature.

I understand the difficulty in defining the parameter. I was hoping that ST could provide some time delay based on a particular circuit scenario. Vout connected directly to some ST ADC over a trace of x width and y length. Certainly, there is some range that can be provided as a rule of thumb.