Skip to main content
smithderek2000
Associate III
Apr 21, 2021 11:17 PM UTC
Solved

What is the temperature sensing accuracy of the LPS22HH for less than 0C?

Hello, according to the datasheet for the LPS22HH, in Table 3 the temperature sensor operating range is -40C to +85C. Further down, it specifies that the temperature sensor absolute accuracy is +/- 1.5C from 0C to 80C.

What is the accuracy from -40C to 0C?

Thanks,

Derek

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Apr 22, 2021 9:52 AM UTC

Hi Derek @smithderek2000​ ,

below 0°C the accuracy is a little worse, probabily because it is more difficult to test in a humidity controlled environment, but nevertheless it is inside +-2.5°C (data from bench measures on representative samples), and almost across all the declared pressure range.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Apr 22, 2021 9:52 AM UTC

Hi Derek @smithderek2000​ ,

below 0°C the accuracy is a little worse, probabily because it is more difficult to test in a humidity controlled environment, but nevertheless it is inside +-2.5°C (data from bench measures on representative samples), and almost across all the declared pressure range.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon