Skip to main content
mart J
Associate
Jun 18, 2018 9:17 AM UTC
Solved

What is the silicon square on the LPS22HB and LPS25HB?

Posted on June 18, 2018 at 11:17

In section 10.1 of the datasheet for the LPS22HB the square on top of the package is labelled as 'Sensing area (exposed silicon)', which makes it sound quite fragile.  However I noticed in a recent press release:

http://www.st.com/content/st_com/en/about/media-center/press-item.html/t4028.html

 the LPS22HB is listed as 'Dust-free and water-resistant by design'.  Is this square of silicon the sensing element or a protective cap (how fragile is it?), and is that the same of the LPS25HB?

Many thanks.

This topic has been closed for replies.
Miroslav BATEKBest answer
ST Employee
Jun 19, 2018 4:33 PM UTC
Posted on June 19, 2018 at 16:33

The sensor LPS22HB is water resistant but not waterproof. Common dust should not be a problem, but if you want to use is in some very dusty area if you recommend to put the sensor in a box wit some filters.

If you need waterproof sensor please use LPS33HW or LPS35HW.

4 replies

ST Employee
Jun 18, 2018 10:02 AM UTC
Posted on June 18, 2018 at 12:02

Yes, the square of silicon is sensing element.

it is not fragile, it is more flexible. 

It is the same as in the LPS25HB.

mart J
mart JAuthor
Associate
Jun 18, 2018 3:42 PM UTC
Posted on June 18, 2018 at 17:42

OK thank you for that information.  Is the sensor dust and water resistant?  I would think any dust on the sensing element will at least affect the readings?

Miroslav BATEKBest answer
ST Employee
Jun 19, 2018 4:33 PM UTC
Posted on June 19, 2018 at 16:33

The sensor LPS22HB is water resistant but not waterproof. Common dust should not be a problem, but if you want to use is in some very dusty area if you recommend to put the sensor in a box wit some filters.

If you need waterproof sensor please use LPS33HW or LPS35HW.

mart J
mart JAuthor
Associate
Jun 19, 2018 7:26 PM UTC
Posted on June 19, 2018 at 19:26

Thank you Miroslav.  The environment I want to use this in isn't especially dusty so it sounds like this sensor will be OK for me. 

Thanks again.