Skip to main content
JG.2
Associate II
April 5, 2022
Question

What is the reason for Rapid increase of Temperature in STM32MP157AAD3?

Our board is similar to STM32MP157C-DK2 Disco board - All the Developer packages has been installed, After providing required functional voltages board's temperature rises rapidly as well as exponentially. After certain temperature there is some abnormal functional activities in the board. What is the reason and solution for the issue faced?

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
April 5, 2022

Hi @JG.2​ ,

It is normal to have some heat from the STM32MP157AAD3, depending on activity.

If your board heating much more than DK2 board, I will suspect an HW issue.

Please check the source of the heat (using fingers or thermal camera), it could be from another component on your board.

Check power supply levels Vs datasheet.

If issue on only one board, please check for manufacturing issues (reversed component, short-circuit, open-circuit, etc...).

Please check very very carefully and thoroughly your schematics and ballout for STM32MP157AAD3 Vs product datasheet and AN5031.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
JG.2
JG.2Author
Associate II
April 5, 2022

Thanks for your response @PatrickF​ we will have a close look over it.