Skip to main content
NSemrHomeInit
Associate III
March 23, 2023
Solved

What is the purpose of VDDIO in ISM330DLC Accelerometer

Dear ST,

I am using the ISM330DLC gyro and accelerometer,

In the electrical connection mode 1 I have a pin called VDDIO.

In my application I connected this pin to 3V but, I don't have any idea what is the use of this pin?

Thank you for explaining

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    March 23, 2023

    Well, that's in the data sheet, table 1, with the pin descriptions:

    VDDIO(1) Power supply for I/O pins

    Footnote 1 stands for: Recommended 100 nF filter capacitor.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    3 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    March 23, 2023

    Well, that's in the data sheet, table 1, with the pin descriptions:

    VDDIO(1) Power supply for I/O pins

    Footnote 1 stands for: Recommended 100 nF filter capacitor.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    NSemrHomeInit
    Associate III
    March 23, 2023

    Hello Peter,

    I think that means If I want 4.5v on INT1/2, went the interrupt is triggered, I have to connect VIO to 4.5v?

    Peter BENSCH
    ST Technical Moderator
    March 23, 2023

    The data sheet clearly states in Table 3:

    Vdd_IO = Power supply for I/O, min 1.62V, max 3.6 V

    4.5V are slightly above 3.6V, so they are not permitted.

    If you need a different voltage level because the connected components work there, you still have to keep within the voltage range for VDDIO and use a level shifter at INT1 or INT2, for example.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.