Skip to main content
MHass.2
Associate II
March 21, 2021
Question

What is the maximum range of SPI communication protocol ?

Hi,

I want to use accelerometer using stm32f4 mcu with SPI protocol.

The range is between 1 and 2 meters. Is this work good ?

Thanks...

This topic has been closed for replies.

3 replies

Pavel A.
March 22, 2021

SPI over 2 meters? No way, without extender

-- pa

Winfred LU
ST Employee
March 22, 2021

Technically you may do that but it will not be a trivial task.

The maximum possible length of SPI line at a specific clock frequency is limited by the phase delay between CLK and MISO seen by the master.

Line driver may be required. Typical issues of a long transmission need to be taken care: impedance matching, inductive noise, etc.

Ozone
Principal
March 22, 2021

As mentioned, for high speed, you would need impedance-matched lines and transceivers.

However, most accelerometers have a relatively low bandwidth, I guess 1ksps or less would do for your purpose.

You can reduce the SPI clock frequency, to ease the line requirement.

About 100 ... 200kHz should suffice.