Skip to main content
JTomp.1
Associate II
November 24, 2021
Solved

What is the I2C bus capacitance of LIS2MDL and LSM6DSL?

I have both these devices on the same I2C bus and am trying to calculate the maximum pullup resistance.

Thanks!

    This topic has been closed for replies.
    TBomb.1
    TBomb.1Best answer
    Visitor II
    November 26, 2021

    Hi, usually they are driven or left at high impedance, so the capacitance is mostly determined by the parasitic of the pcb on the I2C lines.

    Pay attention to the max I2C speed. I believe you can go up to 100kOhm pullup, if you want to minimize the consumption.

    \Tom

    2 replies

    TBomb.1
    TBomb.1Best answer
    Visitor II
    November 26, 2021

    Hi, usually they are driven or left at high impedance, so the capacitance is mostly determined by the parasitic of the pcb on the I2C lines.

    Pay attention to the max I2C speed. I believe you can go up to 100kOhm pullup, if you want to minimize the consumption.

    \Tom

    ASbor.1
    Visitor II
    August 17, 2022

    Hello All!

    Is it possible to interrogate 30 sensors through the I2C expander without using an interrupt

     - LIS2MDL ? I can attach the diagram in the next message if necessary.