Skip to main content
esakkiraja
Associate
December 17, 2016
Question

what is the exact principle of time of flight technology?

Posted on December 17, 2016 at 06:48

Hi, i searched for the exact principle of the time of flight technology in internet but the answer i got was different in different websites. I bought VL53l0X sensor recently and i need the exact principle of TOF of ST's product.

    This topic has been closed for replies.

    2 replies

    Seb
    ST Employee
    December 17, 2016
    Posted on December 17, 2016 at 07:10

    Most of the information is in the

    http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/b2/1e/33/77/c6/92/47/6b/DM00279086/files/DM00279086.pdf/jcr:content/translations/en.DM00279086.pdf

    :

    Burst of infrared pulses from vertical laser is emitted in a cone shaped solid angle.

    If there is an object, the reflected light beam will be sensed by the avalanche photo diod.

    The distance is calculated by mesuring the time it took from emission to reception of a light pulse.

    0.299792 mm per picosecond ==> 1mm correspond to ~3 ps time granularity implementation

    esakkiraja
    Associate
    December 17, 2016
    Posted on December 17, 2016 at 07:25

    And also one more doubt on Calibration. Is offset calibration done in any specific ranging mode such as long range, high accuracy and high speed?