Skip to main content
kasi viswanadh
Associate II
June 4, 2019
Question

what is the effect of mechanical shock and vibration on MotionFX sensor fusion library. What can go wrong if mems sensors placed on a cricket bat undergoing 30g force for few millis when ball hits the bat?

MotionFX,LSM6DSM,LSM303AGR,Sensor fusion,Mechanical Shock,Vibration

    This topic has been closed for replies.

    1 reply

    ST Employee
    June 7, 2019

    Hi,

    first of all what is your final applications?

    I see several problems:

    • Most of the sensors has maximum range 16g so they want be able correctly measure 30g
    • I think the acceleration during the hit could be even higher than 30g, it will be very sharp high peak
    • If the sensor is not able to measure correctly the acceleration the sensor fusion won't be able to follow device position
    • The MotionFX is not designed for such a high acceleration so I think I will also filter high peaks