Skip to main content
JEste
Associate
Sep 13, 2019 8:11 AM UTC
Question

What is the difference between LIS2DTW12 and LIS2DW12?

Hi guys,

I'm working on a new hw design and I can't find the difference between these two references.

Thanks in advance,

Kind regards

This topic has been closed for replies.

7 replies

Eleon BORLINI
ST Employee
Sep 13, 2019 2:38 PM UTC

Hi @Jairo Estefanía​ , the fundamental difference between the two part numbers is the focus on the temperature sensor of the LIS2DTW12 (T stands for "temperature sensor"). Moreover, the LIS2DTW12 has a lower noise density. These two improvements results in a slightly higher current consumption. Basically the LIS2DTW12 is the upgrade of LIS2DW12, so I suggest you the use of the LIS2DTW12. Regards

JasonRrrr
Associate II
Apr 11, 2024 11:05 AM UTC

Is it true that the LIS2DW12TR has lower noise density than the LIS2DW12 ?

 

The figures in the datasheets are exactly the same.

 

JEste
JEsteAuthor
Associate
Sep 16, 2019 6:19 AM UTC

Thanks @Eleon BORLINI​, basically the problem is that there is not enough stock of LIS2DTW12, so we will have to use the LIS2DW12.

Eleon BORLINI
ST Employee
Sep 16, 2019 9:12 AM UTC

I understand. How many samples do you need if I can ask? Regards

JEste
JEsteAuthor
Associate
Sep 16, 2019 9:52 AM UTC

@Eleon BORLINI​  about 12k

Eleon BORLINI
ST Employee
Sep 16, 2019 10:04 AM UTC

Depending on your specific application, I would believe LIS2DW12 should work as well, because the two pn are very similar. Regards

STLearner
Associate III
Jun 4, 2025 6:51 AM UTC

Hi @Eleon BORLINI ,

Both parts seem to have the temperature sensor and having the same pinpout/configuration.

 

Can we read the temperature information from LIS2DW12?