Skip to main content
Pasi MYLLYMAKI
ST Employee
Mar 3, 2021 4:17 PM UTC
Solved

What is the current consumption of Machine Learning running the angle detection algorithm?

..

    This topic has been closed for replies.
    Carlo LARGHI
    Carlo LARGHIBest answer
    Visitor II
    Mar 3, 2021 5:47 PM UTC

    the typical power consumption increase of the sensor when the MLC is used is in the range of few uA, which is almost negligible compared to the power consumption of the inclinometer itself which is in the range of 400uA, and of a microcontroller which, depends of course on the application, but is at least in the range of tens of uA

    1 reply

    Carlo LARGHI
    Carlo LARGHIBest answer
    Visitor II
    Mar 3, 2021 5:47 PM UTC

    the typical power consumption increase of the sensor when the MLC is used is in the range of few uA, which is almost negligible compared to the power consumption of the inclinometer itself which is in the range of 400uA, and of a microcontroller which, depends of course on the application, but is at least in the range of tens of uA