Skip to main content
MVerm.11
Associate
Jan 18, 2021 2:10 PM UTC
Solved

What is the advanced feature of the pull up at pin SA0 of IIS2DH?

We discovered that the SA0 Input of the IIS2DH of your accelerometers has a very high pull up current.

The pull up is about 40 kOhm at IIC adress select line input. If engineers will use two IIS2DH in there design.

Than the IIS2DH at adres 0x18, means SA0 is LOW, then this chip will draw 10 to 15 times the normal operational current. For an extreme low power device. This is a very special feature from ST.

We would like to know:

What is the feature of this pull up

Why is it not specified in the datasheets?

Wil the IIS2DH soon become obselete?

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Jan 19, 2021 7:50 AM UTC

    Hi @MVerm.1​ ,

    the solution you chose is the correct one since it is the safest, I thought you weren't able to modify the circuit and/or you had two different devices sharing the same I2C line. I can say you that setting the MSB of that register (1Eh) can disconnect the internal pullup.

    In my last reply, I forgot to answer to your question:

    >> Will the IIS2DH soon become obsolete?

    This product has been committed by ST for the 10-years product longevity, so the product will not become obsolete soon.

    -Eleon

    3 replies

    Eleon BORLINI
    ST Employee
    Jan 18, 2021 3:06 PM UTC

    Hi @MVerm.1​ ,

    you are right, the pull-up is about that value for Vdd around 2V.

    There could be a solution, however. You could try to disconnect the pull-up by setting '1' the MSB register of the reserved register 1Eh, even if not declared on the datasheet.

    -Eleon

    MVerm.11
    MVerm.11Author
    Associate
    Jan 18, 2021 6:03 PM UTC

    Hi Eleon,

    Thanks for your fast response.

    I did not expect a solution, for this issue, so we had patched the prototypes already to IIC adres 0x19.

    Can you give us the register definition of theis reserve 0x1E? So we can test it.

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Jan 19, 2021 7:50 AM UTC

    Hi @MVerm.1​ ,

    the solution you chose is the correct one since it is the safest, I thought you weren't able to modify the circuit and/or you had two different devices sharing the same I2C line. I can say you that setting the MSB of that register (1Eh) can disconnect the internal pullup.

    In my last reply, I forgot to answer to your question:

    >> Will the IIS2DH soon become obsolete?

    This product has been committed by ST for the 10-years product longevity, so the product will not become obsolete soon.

    -Eleon