Skip to main content
Panometric
Associate III
March 27, 2020
Solved

What is the accuracy of the LSM6DSO timestamp frequency of 40 KHz?

There does not seem to be anything in the datasheet about set tolerance, or drift over temperature. 

https://www.st.com/resource/en/datasheet/lsm6dso.pdf

Assume the INTERNAL_FREQ_FINE is unchanged. It has a step size of .15%, so one would presume the best you can do is around that if it is calibrated.

I am more concerned with the un-calibrated difference, and how that might change over temp.

Thanks.

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    March 30, 2020

    Hi @Panometric​ , the 40kHz frequency is directly related to the max ODR 6.66kHz: a single data set is composed of 6 data (3 axis accelerometer + 3 axis gyro), so ODR_max x 6 = 40kHz. The INTERNAL_FREQ_FINE is a read-only register and is related to the factory calibration: it's value (step size 0.15%) is related to the jitter ("accuracy"), and has to be related to the ODR currently used. The ODR vs temperature change, from characterization data, is about the same order of magnitude. Regards

    2 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    March 30, 2020

    Hi @Panometric​ , the 40kHz frequency is directly related to the max ODR 6.66kHz: a single data set is composed of 6 data (3 axis accelerometer + 3 axis gyro), so ODR_max x 6 = 40kHz. The INTERNAL_FREQ_FINE is a read-only register and is related to the factory calibration: it's value (step size 0.15%) is related to the jitter ("accuracy"), and has to be related to the ODR currently used. The ODR vs temperature change, from characterization data, is about the same order of magnitude. Regards

    AMoul
    Associate II
    November 22, 2022

    Eleon, I think you're missing the point. The question is about accuracy and stability.The device's internal clock frequency equation should include spec on toleranced and temerature drift etc which is totally missing in the datasheet. It's as if the document was written by the software guys. Has ST acually characterised the clock performance?