Skip to main content
User_of_Sensor
Associate
November 4, 2019
Question

What is Nonlinearity (Range: +/- 16g) of the IIS2DLPC acceleration sensor ? Cannot find in the data sheet of IIS2DLPC.

..

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
December 5, 2019

Hi @User_of_Sensor​ , sorry for the delayed answer. Please note that the Nonlinearity parameter is not commonly found in datasheets, because it is closely related to the target application. Which is yours? For a better understanding of the test, a sine vibration is applied to the DUT by sweeping in amplitude with integer step equal to 1g, from 1g to 15g and step 0.2 g from 15.2g to 16g.

  • On X axis, a typical max NL value is 0.63%FS
  • On Y axis, a typical max NL value is 0.81%FS
  • On Z axis, a typical max NL value is 0.60%FS

Please note that these are only indicative values from characterization, since they are not in the datasheet.

Regards