Skip to main content
Evelina CAMILLERI
ST Employee
April 4, 2022
Solved

What is clock frequency of finite state machine located on the MEMS sensor?

..

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    April 4, 2022

    Considering the clock frequency in this question as the rate the FSM processes data, there are four available data rates in LSM6DSOX: 12.5 Hz, 26 Hz, 52 Hz, 104 Hz.

    The FSM data rate can be chosen in Unico-GUI when building the FSM, or alternatively configured through the FSM_ODR1 and FSM_ODR0 bits in the EMB_FUNC_ODR_CFG_B (5Fh) register of the LSM6DSOX.

    1 reply

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    April 4, 2022

    Considering the clock frequency in this question as the rate the FSM processes data, there are four available data rates in LSM6DSOX: 12.5 Hz, 26 Hz, 52 Hz, 104 Hz.

    The FSM data rate can be chosen in Unico-GUI when building the FSM, or alternatively configured through the FSM_ODR1 and FSM_ODR0 bits in the EMB_FUNC_ODR_CFG_B (5Fh) register of the LSM6DSOX.