Skip to main content
SG.8
Visitor II
February 20, 2022
Solved

What is best PCB material for IIS3DWB accelerometer for industrial condition monitor? Is there any ST recommended guideline for PCB layout and fabrication?

..

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    February 28, 2022

    Hi @SG.8​ ,

    we suggest a board form factor such as the STEVAL-MKI208V1K, a standard FR4 1.6mm board which is optimized for minimizing its own vibrations.

    This design, differently from the DIL 24 standard adapter, can be connected through a flat cable to the application board (such as a custom board or theSTWINKT1B reference design).

    For a clean monitoring of a vibrating object, the spurious mechanical vibrations of the application board must be disentangled by the vibration of the system under test.

    You can find more information (together with an overview of the firmware tools dedicated to the vibration monitoring) here: Vibration Monitoring using IIS3DWB Vibration Sensor - STMicroelectronics

    Moreover, as a general guideline for mounting the device on the board, you can refer to this tech note: TN0018 Technical note - STMicroelectronics

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

    -Eleon

    1 reply

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    February 28, 2022

    Hi @SG.8​ ,

    we suggest a board form factor such as the STEVAL-MKI208V1K, a standard FR4 1.6mm board which is optimized for minimizing its own vibrations.

    This design, differently from the DIL 24 standard adapter, can be connected through a flat cable to the application board (such as a custom board or theSTWINKT1B reference design).

    For a clean monitoring of a vibrating object, the spurious mechanical vibrations of the application board must be disentangled by the vibration of the system under test.

    You can find more information (together with an overview of the firmware tools dedicated to the vibration monitoring) here: Vibration Monitoring using IIS3DWB Vibration Sensor - STMicroelectronics

    Moreover, as a general guideline for mounting the device on the board, you can refer to this tech note: TN0018 Technical note - STMicroelectronics

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

    -Eleon