Skip to main content
Associate
September 25, 2023
Solved

What do the self-tests of the ASM330LHH actually prove?

Hello, I hope you are well.

I had a query about the IMU ASM330LHH. I want to know whether the self-test functions of the internal accelerometer and gyroscope (see attached pictures) test the internal MEMS sensors or not. I have doubts whether these self-tests only internally generate standard values for acceleration and angular velocity without actually testing the MEMS.

Thank you very much.

This topic has been closed for replies.
Issamos
IssamosBest answer
Super User
September 25, 2023

Hello @FedIng 

The embedded self-test functions allow checking the device functionality without moving it.

Also, When the accelerometer self-test is enabled, an actuation force is applied to the sensor, simulating a definite input acceleration. In this case, the sensor outputs exhibit a change in their DC levels which are related to the selected full scale through the sensitivity value.

The accelerometer self-test function is off when the ST[1:0]_XL bits of the CTRL5_C register are programmed to 00. It is enabled when the ST[1:0]_XL bits are set to 01 (positive sign self-test) or 10 (negative sign self-test). When the accelerometer self-test is activated, the sensor output level is given by the algebraic sum of the signals produced by the acceleration acting on the sensor and by the electrostatic test-force.

For more informations about the self-test, take a look at the chapter 9 of the AN5296.

Best regards.

II

2 replies

Issamos
IssamosBest answer
Super User
September 25, 2023

Hello @FedIng 

The embedded self-test functions allow checking the device functionality without moving it.

Also, When the accelerometer self-test is enabled, an actuation force is applied to the sensor, simulating a definite input acceleration. In this case, the sensor outputs exhibit a change in their DC levels which are related to the selected full scale through the sensitivity value.

The accelerometer self-test function is off when the ST[1:0]_XL bits of the CTRL5_C register are programmed to 00. It is enabled when the ST[1:0]_XL bits are set to 01 (positive sign self-test) or 10 (negative sign self-test). When the accelerometer self-test is activated, the sensor output level is given by the algebraic sum of the signals produced by the acceleration acting on the sensor and by the electrostatic test-force.

For more informations about the self-test, take a look at the chapter 9 of the AN5296.

Best regards.

II

FedIngAuthor
Associate
September 26, 2023

¡Thank you so much @Issamos for the complete answer and the AN link!