Skip to main content
jg_spitfire
Senior
June 3, 2020
Solved

what are the function of DEN_A/G and DRDY_M pins of LSM9DS1?

Hi, the datasheet does not provide enought info about when to use or the benefits of use this pins, does anybody has used it?

thanks

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    June 4, 2020

    Hi @jg_spitfire​ ,

    • the DEN_A/G pin can be used as data ready output for the accelerometer/gyro part of the module: its purpose is to synchronize the measurement with external signal, and if you don't need this functionality you can keep i unconnected. To enable this functionality you have to configure it in the proper registers, but you can use as well the INT1 and INT2 pins.
    • the DRDY_M is the magnetometer subchip data ready output (that goes up when the magnetometer data is available, if properly configured), and has the same functionality as the DEN_A/G of the accelerometer/gyro but for the magnetic sensor.

    These pins can appear quite not useful, but are used for debug and test mode purposes.

    Regards

    2 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    June 4, 2020

    Hi @jg_spitfire​ ,

    • the DEN_A/G pin can be used as data ready output for the accelerometer/gyro part of the module: its purpose is to synchronize the measurement with external signal, and if you don't need this functionality you can keep i unconnected. To enable this functionality you have to configure it in the proper registers, but you can use as well the INT1 and INT2 pins.
    • the DRDY_M is the magnetometer subchip data ready output (that goes up when the magnetometer data is available, if properly configured), and has the same functionality as the DEN_A/G of the accelerometer/gyro but for the magnetic sensor.

    These pins can appear quite not useful, but are used for debug and test mode purposes.

    Regards

    jg_spitfire
    Senior
    June 4, 2020

    thanks!