Skip to main content
davidle.ee9
Associate II
April 30, 2019
Question

What are the differences and advantages between the LIS2DH12 and LIS2DW12 ?

What are the differences and advantages between the LIS2DH12 and LIS2DW12 ?

Please let me know if I do want to use this sensor for detection the device is not moving in any directions (NO MOTION) at very low current consumption then which ONE i should pick.

Thanks

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    May 3, 2019

    Hi davidle, I would suggest you to use the LIS2DW12 for the following reasons: first, it's a newer product and will be of course supported for longer time; second, for your application (movement detection), if you don't want to have a fine detection of high-frequency movements (fast or harsh movement, for example), you can set low ODRs, e.g. working in low power (12.5Hz or 10Hz ODR, LP) the current consumption is lower than LIS2DH12, down to 1uA consumption.; third, is more stable vs temperature. Can you work in low power mode in your app? Regards

    davidle.ee9
    Associate II
    May 3, 2019

    Yes I will use the LIS2DW12 in low ODRs to get 1uA consumption.

    Thanks