Skip to main content
fabiano
Visitor II
July 15, 2016
Question

wesu board drift

Posted on July 15, 2016 at 12:08

Hello,

I just received the wesu board and I using it ''as it is'' with the related android app ST WeSU.

What I'm facing looking at the cube on the app is that there is a very high drift of the cube itself.

In details:

if I move the board I see the cube moving coherently but when I put the board in a stable fixed position I see that cube take a very long time (up to 10/12 seconds, depending on the previous movements) to reach a fixed stable position.

What could be the root cause?

Thanks in advance

Fabiano

#wesu-drift
This topic has been closed for replies.

1 reply

louda.marian
ST Employee
July 22, 2016
Posted on July 22, 2016 at 15:11

Hello,

I have observed the same behavior.

It is a matter of fusion library. Lite version of fusion library is used in firmware of WeSu.

Best Regards,

Marian