Skip to main content
JMola.1
Associate
September 23, 2020
Question

We see a high variation in LPS33HW outputs. These are factory calibrated to 0.1 hPa, but we are seeing +/-3 hPa. Do we have to do anything specific at power up to apply the factory trimming values?

  • September 23, 2020
  • 2 replies
  • 745 views

We are using two sensors. One is attached to a patient breathing circuit and the other is set to ambient pressure. We display the differential.

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    September 25, 2020

    Hi @JMola.1​ ,

    do you see the same variation on both sensors you are using? Or the +/-3 hPa is the differential pressure between the two sensors?

    The factory calibration values are loaded in register just after the device power-up, and after that you have to

    /*
     * Restore default configuration
     */
     lps33hw_reset_set(&dev_ctx, PROPERTY_ENABLE);
     do {
     lps33hw_reset_get(&dev_ctx, &rst);
     } while (rst);
     /*
     * Enable Block Data Update
     */
     lps33hw_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
     /*
     * Set Output Data Rate
     */
     lps33hw_data_rate_set(&dev_ctx, LPS33HW_ODR_10_Hz);

    I suggest you to check the read_data_simple.c file on Github repository.

    To increase the accuracy, and if you are interested in differential pressure (i.e. the pressure variation with respect to a reference pressure), you may use the Autozero function described in the datasheet, p.34, and implemented in C code in the github drivers (lps33hw_reg.c).

    -Eleon

    JMola.1
    JMola.1Author
    Associate
    September 25, 2020
    Eleon,
    Thank you for the response.
    None of the sensors read accurate barometric pressure in our testing against a NIST calibrated instrument. Individually they read +/-3 hPa. When paired we have seen differences as large as 5 hPa.
    We will look at the Git Hub information and the code you show below and get back to you.
    Regards,
    John