Skip to main content
ANANTH
Associate
August 21, 2020
Question

we have chosen vl53l0x for our product. Before that we bought x nuculeo expansion board and tested(without cover glass),everything is working fine.But after placing cover glass , the sensor first gave measurement as 0mm always.

Then we tried to do calibration steps as per datasheet, but the offset we are getting is -25000(we placed the white object at 100mm) and cross talk is 0.

SOC : nrf52840

RTOS : Zephyr

GITHUB link for driver : https://github.com/zephyrproject-rtos/hal_st

My doubt is on driver where it is doing calibration for offset and cross talk

Line number 141 in this file, https://github.com/zephyrproject-rtos/hal_st/blob/master/sensor/vl53l0x/api/core/src/vl53l0x_api_calibration.c ,xTalkCalDistanceAsInt will become 0 because

it is shifted by 16 places.If this is the problem then so many places it is happening.

Can anyone help me solve this problem.Thanks in advance.

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
August 26, 2020

The hardware works in 10.2 format. that is if an offset is 25mm the hardware would give 25<<2. So two binary bits to the right of the implied binary point. (Almost like a decimal point, but in base 2).

However in the ST code someone thought that was odd, and though it would be easier for people to think in thousandths. So the multiplied the 25<<2 by 250 to give thousandths of millimeters - or micrometers.

The code is self-consistent. That means if you do the calibration and get a number, and then put that number back through the same set of software, it will work - even though the number looks odd.

To get a number that makes sense simply divide that number by 1000 and you get the offset in millimeters.

a -25mm is a very typical offset, even though it got left shifted by 2 and then multiplied by 250.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
ANANTH
ANANTHAuthor
Associate
August 27, 2020

what about this line for cross talk https://github.com/zephyrproject-rtos/hal_st/blob/5b3ec3e182d4310e8943cc34c6c70ae57d9711da/sensor/vl53l0x/api/core/src/vl53l0x_api_calibration.c#L141 where xTalkCalDistanceAsInt becomes 0(because of shifting) and following condition(xTalkStoredMeanRange >= XTalkCalDistance) becomes true always, so i am getting 0 always.Is this also correct?