Skip to main content
ATorb.1
Associate
May 18, 2021 9:33 PM UTC
Solved

We evaluated a MKI209V1 Dev Kit using the Unico-GUI software and now I want to talk to it directly from a PC (still using the Dev Kit). I found the Unico-Lite Example software. Any examples of talking to MKI209V1 from Unico-Lite, or any C# examples?

..

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
May 20, 2021 8:09 AM UTC

Hi @ATorborg​ ,

since the MKI209V1 device is an accelerometer, the suitable commands are the ones related to accelerometer sensor.

For completeness, you can find the list of supported command in Table 2 and Table 3 of the user manual UM2116, p.12.

*setdb209V1 // recognize the proper adapter
[ *r0F // read WHO_AM_I register
*w1060 // write ODR 104Hz, FS 2g and NM operationg mode in CTRL1_XL (10h)]
*start //run continuous data acquisition

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon

4 replies

Eleon BORLINI
ST Employee
May 19, 2021 3:23 PM UTC

Hi @ATorborg​ ,

yes, you can use the commands described in the Unico GUI lite software user manual, that can be send via VCOM and can be managed by an high-level software in an automatized routine.

For example:

*rAA // For reading accelerometer data
*grAA // For reading gyroscope data
*mrAA // For reading magnetometer data
*prAA // For reading barometer data

After the command is sent, the board replies with the register value: an example of the string format is “RAAhVVh�?, where AA is the address and VV is the value.

Can it be enough for your scope?

-Eleon

ATorb.1
ATorb.1Author
Associate
May 19, 2021 6:29 PM UTC

Hi Elean - Thanks for the reply. For starters, if I add the MK1209V1, what does I use for the "words" and "dbset" values? Thanks,Alan

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
May 20, 2021 8:09 AM UTC

Hi @ATorborg​ ,

since the MKI209V1 device is an accelerometer, the suitable commands are the ones related to accelerometer sensor.

For completeness, you can find the list of supported command in Table 2 and Table 3 of the user manual UM2116, p.12.

*setdb209V1 // recognize the proper adapter
[ *r0F // read WHO_AM_I register
*w1060 // write ODR 104Hz, FS 2g and NM operationg mode in CTRL1_XL (10h)]
*start //run continuous data acquisition

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon

ATorb.1
ATorb.1Author
Associate
May 20, 2021 5:08 PM UTC

I think this was enough to get me started - thanks Eleon