SAlug.1Associate II5 years agoJuly 26, 2021QuestionWe are using accelerometer ISM330DLC to find the Motor Frequency, Instead of 800Hz we are getting peak at 2KHz4 replies4160 viewsWe are Reading Accelerometer Raw Data from the sensor and plotting FFT on excel sheet The ODR was configured to 6660(6.66Khz)Each Time we are reading 256 points of X, Y , Z Plz find the attachment for more details The Motor is running at 800Hz we are observing peak at 2KHz . Not sure why we are getting wrong FFT plot .Can you help why I am getting wrong FFT Plot.Sensor_data.xlsxAccelerometers