Skip to main content
Cc l.1
Visitor II
August 11, 2020
Question

We are using 6 axis sensor part no-LSM6DSOTR for battery operated device . We are Supplying 3.3V for VDD and VDDIO ,In Data Sheet Current Consumption Is Mentioned for 1. 8V .We would Like Know the Current Consumption for 3.3V. Thanks in advance..

..

    This topic has been closed for replies.

    1 reply

    niccolò
    ST Employee
    August 12, 2020

    Hi @Cc l.1​,

    to provide you with typical values of power consumption I would need to know which power mode you are using, and if you are turning on both accelerometer and gyroscope or just one of the two.

    best regards.