Skip to main content
Nickname2530_O
Visitor II
June 24, 2014
Question

VL6180X: What is the linearity error rate ?

Posted on June 24, 2014 at 09:43

Dear,

What is the linearity error rate with VL6180X ?

Tks and regards.

A.

#proximity-sensor #vl6180x
This topic has been closed for replies.

2 replies

Colin RAMRATTAN
Visitor II
June 24, 2014
Posted on June 24, 2014 at 17:51

Hello Augustin,

The VL6180X can measure all reflectances of material from 0 to 100mm with a measurement tolerance of +/- 10mm. However, if range offset calibration is not performed in the end application, this could increase to +/- 13mm. If range offset calibration is performed in the end application the original +/- 10mm measurement tolerance can be achieved.

Now, to answer your question, there is no specific linearity error equation that can be provided for the VL6180X. The measurement tolerance has been stated clearly in the datasheet under page 35.

Jeffrey Will
Visitor II
June 16, 2017
Posted on June 16, 2017 at 02:44

I'm also seeing quite a non-linearity.  It is repeatable.  My calibration data is:

Actual mmSensor 1Sensor 2

13148

252724

383938

515052

646265

767276

898188

1028999

If +/ 10 mm is what I can expect, that's ok.  But page 35 of the datasheet seems to say that noise is 2 mm, offset is 13 mm (can be compensated for), drift is 15  and 5 (mine does not drift day to day).

I was hoping for better performance than +/- 1 cm.  Am I asking too much?